Meistgelesene Industrie-Blogthemen, die 2021 veröffentlicht wurden
-
Tale of 4 Costs
For companies that were already following a path to digital transformation, the sudden shift brought on by the pandemic was not as jarring and the change affirmed that they were headed in the right direction. For industrial sites that weren't yet taking advantage of automation, the writing was on the wall: change is here, and it's here to stay. When it comes to total cost of ownership for industrial-grade cables, this blog walks through four factors to consider.
- Die wichtigsten Herausforderungen für IT/OT: Hören Sie von den Experten
In this blog, we spoke with experts in the field who offered their insights about the challenges facing IT and OT convergence. When you think of Information Technology (IT) and Operational Technology (OT), which side are you on? You may not feel that you fall on any side of that technological skirmish, but when you stop to carefully consider the differences in these two disciplines, it is nearly impossible to avoid a tendentious leaning.
- Mit TSN das Gesicht der Automatisierung verändern
Thanks to Industry 4.0 (also referred to as the "smart factory"), digital technology has become a priority for the manufacturing industry over the past few decades. This change offers enhanced visibility and connectivity between the sensors on the factory floor and the factory backbone, allowing data to move through at high speeds and to be available where it is needed for value-add services such as data analytics. This blog dives into how digital technology has taken over many aspects of our lives on and off the factory floor.
- Form A, B und C: Kennen Sie Ihre DIN-Ventilsteckverbinder?
Überall, wo es Fertigungsprozesse gibt, werden auch DIN-Ventilsteckverbinder eingesetzt. They're used in automotive, chemical, food/beverage, pharmaceutical, oil/gas and water/wastewater environments, to provide just a few examples. Learn about the three standard types of DIN valve connectors in this blog.
- Merging Tray Cable with M12 Power Technology for New Uses
This blog explains how the combination of tray cables and M12 connectivity is valuable not only in automotive applications, but also in applications that need to supply power to motors on a conveyor belt system, as well as power supplies, power converters and the industrial lighting industry.
Most-Read Belden Industrial Blogs Ever
These five blogs were published before 2021 and have proven to be the most popular among our viewers.
- Managed vs. Unmanaged Switches - Are they Really that Different?
Comparing managed and unmanaged switches is almost like comparing today's smartphones with your very first 1990s mobile phone. Beide Geräte dienen demselben grundlegenden Zweck – der Sprachkommunikation – aber da endet jede Gemeinsamkeit. Ihre Anwendung bestimmt, welche Art von Switch Sie benötigen. Learn which type of switch is right for you in this 2020 blog.
- RS-485-Kabel: kritisch für den Systembetrieb
This 2018 blog discusses cable options as well as distance details for the RS-485 cable. It is important to remember that EIA-485 is not an application or protocol but a balanced transmission interconnect standard that specifies the electrical characteristics of drivers, receivers and transceivers.
- 600V Industrial Ethernet Cable: Safety & NEC Considerations
When Ethernet cable is used in such a 600-volt environment, electrical safety becomes a design consideration. The challenge is that Ethernet products have not traditionally been offered in a form that easily integrates with industrial machinery AND conforms to safety regulations. If you suspect that your 600V Ethernet application needs to conform to the NEC regulations, or if you simply want to understand 600V cable safety considerations, read on.
- Tipps für den korrekten Anschluss von VFD-Kabeln
This blog discusses how the population of variable frequency drives in modern industrial facilities has escalated significantly in recent years. And no wonder-by adjusting motor speed and voltage to meet changing real-time process demands on the fly, VFDs help deliver valuable benefits such as increased energy efficiency, more precise process control and reduced wear and tear on costly equipment. This blog offers tips that can help you properly terminate your VFD for system reliability.
- Kabel für die direkte Erdverlegung: Ihre Fragen werden beantwortet
Bei der Verlegung von Kabeln unter der Erde – und der Sicherstellung einer kontinuierlichen Leistung trotz der Hindernisse, auf die sie stoßen können – sind einige Fragen zu berücksichtigen. Möchten Sie Kabelkanäle verlegen? Ist Feuchtigkeit ein Problem? Is the cable running across long distances? This 2020 blog covers the 3 cable types that normally rise to the surface in discussions about outdoor installation.
Thank you for continuing to read Belden’s blogs – and for sharing your feedback, comments and ideas. Don’t forget to subscribe to our blogs
here!