Intelligentes Gebäude

Patch Cord Types and Their Impact on the Network

Dan Bodenski

Data centers and the networks they support have grown to be an integral part of every business. The software applications that keep mission-critical operations up and running in highly redundant, 24/7 environments rely on highly engineered structured cabling systems to connect the cloud to every user. Structured cabling is the foundation that supports data centers.


Although structured cabling isn’t as sexy as diesel-driven UPS systems or adiabatic cooling systems, it plays a huge role in supporting the cloud. One important component of structured cabling that is often overlooked: patch cords.

 

Oftentimes, patch cords are purchased haphazardly and installed at the last minute. But the right patch cord type can improve the performance of your network. The proper design, specification, manufacturing, installation and ongoing maintenance of patch cord systems can help ensure that your network experiences as much uptime as possible.

 

A patch cord problem can wreak havoc on an enterprise, from preventing an airline customer from making a necessary reservation change to keeping a hotel guest from getting work done while on business travel.

 

What Drives Data Growth?

Explosive data growth due to social media, video streaming, IoT, big data analytics and changes in the data center environment (virtualization, consolidation and high-performance computing) means one thing: Data traffic is not only growing in bandwidth, but also in speed.  

 

Another essential point is network design. Today’s network design, such as a leaf-spine fabric, makes the network flatter, which lowers latency – this makes the Ethernet and corresponding patch cord types incredibly important.

 

The Definition of a Patch Cord

A patch cord is a cable with a connector on both ends (the type of connector is a function of use). A fiber patch cord is sometimes referred to as a "jumper." 

 

Patch cords are part of the local area network (LAN), and are used to connect network switches to servers, storage and monitoring portals (traffic access points). They are considered to be an integral part of the structured cabling system.

 

Copper patch cords are either made with solid or  stranded copper; due to potential signal loss, lengths are typically shorter than connector cables.

 

A fiber patch cord is a fiber optic cable that is capped at both ends with connectors. The caps allow the cord to be rapidly connected to an optical switch or other telecommunications/computer device. The fiber cord is also used to connect the optical transmitter, receiver and terminal box.

 

Selecting Copper Patch Cords

There are many copper patch cord types to consider – but here are a few key elements to keep in mind.

  1. Size: A copper patch cord with a smaller OD (outside diameter) takes up less space, and also has a smaller bend radius. This allows it to be deployed in space-deprived environments, and offers more working space for potential expansion in the future.

  2. Twinning: A stable and consistent twinning process (the twisting of copper conductors) helps maintain internal cable characteristics and reduce signal loss during physical manipulation.

  3. Bonded-Pair Technology: The process of bonding individual conductors along the longitudinal axis guarantees uniform spacing between the twisted pair, as well as reliable electrical performance.

  4. Types of Testing: Transmission performance depends on the integrity of the system, including cable characteristics, connecting hardware, cross-connect wiring and patch cords. Manufacturer testing and post-installation testing ensure that the network remains reliable and 100% available.

  5. Length: Pay attention to length restrictions for twisted pairs.

  6. Connections: Look for snagless, over-molded engineered boots, which offer strain and pull relief to protect patch cords from damage.

  7. Traceability: Having the ability to trace a patch cord’s connection points improves reliability, reduces troubleshooting time, improves uptime and reduces IT teams’ efforts when making changes.

 

Selecting Fiber Patch Cords

Choosing fiber patch cords requires just as many considerations as choosing copper patch cord types. Before selecting a fiber patch cord, ask yourself:

  1. Which connector type is needed? LC, SC, ST, FC, MPO or MTP? Each connector option offers pros and cons. Selecting the right connector can speed up deployment and reduce costs.

  2. Should singlemode or multimode patch cord types be used? Singlemode patch cords are used for long distances; multimode patch cords are used for shorter distances.

  3. Are simplex (one connector per end) or duplex (two connectors per end) cable connections necessary?

  4. How long should the patch cord be? For example, fiber patch cords are available in lengths of 2 m, 3 m or 5 m. The right patch cord length will eliminate slack and potential damage due to kinking.

  5. What type of cable jacket is needed? Depending on the installation location (plenum, underfloor, exterior or floor mounted), the exterior cabling jacket is available in a variety of configurations to protect the cable’s insulation and conductor core. Selecting the right jacket – single jacket, plenum rated, double jacket/armored, double jacket/heavy duty, etc. – for the right environment will ensure proper performance.

The demand for higher bandwidth and faster network speeds requires a network that can handle higher compute densities without sacrificing reliability.

 

Selecting, installing and maintaining the right patch cord type affects today’s network in many ways. Belden’s copper and fiber patch cords offer superior performance and engineered resiliency to meet the bandwidth and network speeds of today, tomorrow and beyond.