Industrielle Kabel für Öl- und Gasprojekte
From subsea drilling 6,000 feet below the surface to pipelines that cross many landscapes to intense refining processes, the range of conditions for oil and gas installations is very broad. Als Konstrukteur können Sie an vielen Arten von Projekten mit sehr unterschiedlichen Anforderungen beteiligt sein. Wie gehen Sie dann bei der Auswahl des richtigen Kabels für eine Öl- und Gasanwendung vor?
But won't any cable do? Certainly not! Cable issues account for more than 70% of signal transmission issues and they are difficult to diagnose and resolve. With downtime costing thousands of dollars per hour, availability requirements demand that the right cable is specified for each use.
The good news is that despite the broad range of oil and gas applications many of them share common cable requirements. In this article I take away the voodoo and spell out the 3 easy steps to selecting the right cable.
1. Select the Right Industrial Cable Jacket
As a resident of the Pacific Northwest I know that snowboarding is fun when I have the right layers on and walking my dog in a downpour is okay when I am in water repellent outerwear from head to toe. Having the right outerwear, or jacket, is also the key to signal reliability for oil and gas applications.
Thus the first question to ask yourself is "How harsh is the environment for my project?" The answer to this leads to selecting the right industrial cable jacket.
The table below categorizes various types of oil and gas applications according to a harsh, harsher, harshest model and indicates the type of cable jacket suitable for each.
Harsh | Harsher | Harshest | |
---|---|---|---|
Beschreibung |
The environment is generally contained but is a true industrial setting |
The environment includes exposure to outside elements and some harsh chemicals |
The environment is exposed to harsh outdoor elements, very harsh chemicals or some other extreme conditions |
Application Example |
Natural gas compressor station:
|
Petrochemical processing facility:
|
Offshore natural gas and oil platform or Onshore drill rig or Onshore pump jack:
|
Suitable Cable Jackets |
|
|
|
2. Select the Level of Oil Resistant Cable Needed
Now that you have narrowed down the range of suitable jacket types, what level of oil proof cable do you need? Will the cable be exposed to:
- Infrequent light splashing - Choose an “oil resistant” jacket.
- Periodic oil exposure - Choose a jacket that is “UL Oil Resistant 1”.
- Frequent harsh oil exposure - Choose “UL Oil Resistant 2”.
Use the following chart to narrow down and select the jacket type for your project.
Harsh | Harsher | Harshest | |||||
---|---|---|---|---|---|---|---|
Material der Ummantelung | LSZH (TP) | PVC | TPE | CPE (TP) | XLink LSZH (TS) | FEP | Panzerung |
Sunlight Resistant |
• |
• |
• |
• |
• |
• |
• |
Ölbeständigkeit |
• |
• |
• |
• |
• |
||
UL Oil Res. I | optional |
• |
• |
• |
• |
optional | |
UL Oil Res. II | optional |
• |
• |
• |
• |
optional | |
Weld Splatter |
• |
• |
• |
||||
Extra Low Temp. |
• |
• |
• |
• |
optional | ||
Extra High Temp. |
• |
||||||
Low Smoke Zero Halogen |
• |
• |
|||||
Halogen Free |
• |
• |
optional | ||||
Endlos-Flex |
• |
||||||
direkte Erdverlegung |
• |
• |
• |
• |
• |
||
Maximum Mechanical Protection |
• |
For those of you who like to know what all of the acronyms that describe cable are, here is a summary.
Cable AcronymsDefinitions | |
---|---|
CPE | Chlorinated polyethylene |
PVC | Polyvinyl chloride |
TP | Stands for "Thermoplastic" and means the material can be melted and re-solidified again, such as ice. |
TS | Stands for "Thermoset" and means that a material has been cured so that it cannot be melted. |
TPE | Thermoplastic elastomer |
FEP | Fluorinated ethylene propylene, also know under the brand name of Teflon |
XLPE | Cross Linked polyethylene. Withstands higher voltages, good for longer cable runs. |
3. Special Considerations by Industrial Cable Type
The three most common cable types used in oil and gas applications are Ethernet, VFD and Control and Instrumentation cable. Let's take a look at the unique selection criteria for each.
Ethernetkabel
The key considerations for choosing copper or fiber Ethernet cable are:
- If you have runs of 100 meters you need fiber
- If you need data rates of more than 1GB than you need fiber
- If you need Power over Ethernet then you need copper
Twisted or Bonded-Pair Conductors?
Bonded-pair cables provide resistance to the rigors of installation by utilizing a manufacturing technique that affixes the insulation of the cable pairs along their longitudinal axes so no gaps can develop between the conductor pairs.
Twisted pair cable construction can be susceptible to pair-gapping during installation, as well as impedance mismatches.
Belden has developed proprietary bonded-pair technology that provides:
- Uniform conductor-to-conductor spacing, or centricity due to the absence of gaps between the conductor pairs.
- Superior electrical performance thanks to the uniform centricity. Installation processes, such as bending, pulling and twisting, do not affect the high functioning of this cable.
Twisted pair conductors have gaps which decrease performance. Belden’s patented bonded-pair technology maintains electrical performance even when cable is bent, pulled or twisted.
VFD-Kabel
Many motor systems are used to pump or refine oil and gas. Often these motor systems use Variable Frequency Drives, or VFDs, to precisely control their speed, as doing so greatly reduces both costs and energy consumption. In addition, VFDs also improve process control, reduce manufacturing waste, provide a longer useful life for motors, reduce maintenance and deliver high reliably.
However, there is a downside to VFDs, and that is that they generate disruptive electrical noise in the environment around them that can create problems in the refining or pumping processes. The noise emission can be difficult to track down and eliminate, causing reduced production or downtime.
Proper cable shielding is thus essential for VFD cable, particularly when longer cable runs are required. Choosing well-designed, robust VFD cables ensures motor uptime and reliability of the VFD system and also provides protection for any sensitive instrumentation and adjacent control systems.
A challenge in purchasing VFD cables is that there are no standards for them. Thus it can be difficult to differentiate between minimum construction-grade cable sold as VFD cable and high-performing VFD cable that protects motors and ensures the maximum benefits of a VFD system.
Below is a quick guide to help you differentiate between the two.
Cable Characteristic | Construction-Grade VFD Cable | High-Performance VFD Cable |
---|---|---|
Abschirmung | Copper-tape shielded building wire | Braided shield construction or dual copper tapes |
Isolierung | PVC/nylon insulation | XLPE-Isolierung |
Grounding | 1 full-size or smaller ground conductor | Insulated grounds, shield and drains equivalent to 3 or more conductors at ground potential |
Verseilung | Bare copper, Class B stranding, Low flex | Tinned copper conductors High strand count; High Flex |
Zertifizierung | Not recommended by the manufacturer of your VFDs | Recommended for use by your VFD manufacturer |
Instrumentation and Control Cable
In addition to selecting the right jacket type, as shown in the tables above, the important thing to determine for Instrumentation and Control cables is the type of insulation.
Here are the guidelines:
- For Harsh environments choose PVC or PVC nylon insulation
- For Harsher environments, choose PVC nylon, or XLPE insulation
- For Harshest environments, choose XLPE insulation
The Right Industrial Cables Deliver High Performance and High Availability
Just like I don’t go to the mountains to snowboard without the right clothing layers and protective gear, so you don’t want cable without the right layers and protection.
If you follow the steps in this article:
- Select the right industrial cable jacket
- Select the level of oil resistant cable needed
- Remember the special considerations by industrial cable type:
- Ethernet – copper or fiber, bonded-pair technology
- VFD – choose high performance cable characteristics
- Instrumentation and Control – select the right insulation
You will choose a cable that provides reliable signal transmissions and high availability.
Here are some examples of the 3 types of cables for each level of environmental harshness:
CableType | Harsh | Harsher | Harshest |
---|---|---|---|
Ethernet | Heavy | Upjacket (an extra jacket layer) | Armored PVC or Jacketed XLink |
VFD | XLP, PVC | XLP, CPE | XLP XLink LSZH |
Instrumentation and Control | PVC or PVC Nylon Insulation with PVC jacket | PVC Nylon or XLPE insulation with CPE jacket | XLPE Insulation with XLink LSZH jacket |
Good luck with your projects and I look forward to hearing whether these guidelines help.