Electrical high voltage ground bar on wall.Grounding electric bar.Cables connected to electrical grounding bar,Ground industry for control system.

The terms “grounding” and “bonding” are often confused or misused (e.g., connecting a lug or piece of metal to a data center rack is often thought of as “grounding” the system however, that process actually “bonds” the system).

 

Grounding vs Bonding

Simplistically put, grounding (typically handled by electricians) involves creating an electrical connection to earth ground—essentially, a copper pole driven into the ground enabling electrical utilities to connect to it.

 

Bonding involves connecting to that grounding system and equalizes the ground potential of equipment eliminating static discharge between devices.

 

In a successful grounding and bonding system, electromagnetic interference noise is carried to ground along a shield to protect data from being impacted by noise during transmission. Any metal component of the networking or data center infrastructure should be bonded to the grounding system.

 

Determining who is responsible for installing a grounding and bonding system can be tricky. Some believe integrators and other cabling installers have a responsibility to recognize and understand grounding and bonding systems while others believe the responsibility lies elsewhere (as bonding is done to a grounding system the low-voltage installer isn’t responsible for).

 

We believe it's important for all involved in cabling and connectivity to understand grounding and bonding however, professionals in the telecommunications industry should primarily be focused on ensuring proper bonding.

 

How Bonding Works

The following summary covers a bonding system in a multi-level building.

  • The primary bonding busbar (PBB) is located on the lowest level of a building & is attached to the grounding system (installed by the electrician).

  • From the PBB runs a telecommunications bonding backbone (TBB), essentially a thick-diameter copper wire running up through each floor of the building to reduce variation between telecom systems on different floors.

  • Each floor of the building has a secondary bonding busbar (SBB) which runs continuously to connect all SBBs to the PBB on the lowest level.
  • The cable shielding system attaches to the SBBs & TBBs in the grounding system.

  • If the building has equipment running on each side, the same scenario holds true for the other side of the building.

ANSI/TIA-607-C (Generic Telecommunications Bonding and Grounding for Customer Premises) encourages planning, design and installation of telecommunications grounding and bonding systems in new buildings, renovations or retrofits. Belden bonds cable shields to ensure proper system performance. Additionally, the third prong on all Belden equipment is considered a ground (in scenarios where it has a good path to earth ground).

Über den Autor

Ron Tellas

Senior Solution Architect, Enterprise Solutions, Belden

Ron Tellas ist Fachexperte für HF-Design und elektromagnetische Ausbreitung. Er hat sich Belden im Jahr 2016 angeschlossen, um mitzuhelfen, den Zeitplan für Technologien und Anwendungen im Bereich intelligente Gebäude mitzugestalten. Dank dieser Erfahrungen kann er heute sehr effektiv Systeme, Geräte und Verbindungstechnik in Netzwerklösungen integrieren. Ron Tellas vertritt Belden in mehreren Standardisierungsorganisationen, Ausschüssen des National Electrical Code und als Vorstandsmitglied der FMP Alliance. Er hat einen Master- und Bachelor-Abschluss in Elektrotechnik und einen Master-Abschluss in Betriebswirtschaftslehre erworben und hat 17 US-Patente angemeldet. Er ist stolzer Empfänger des 2024 Harry J. Pfister Award, einer Auszeichnung, die er für seine herausragenden und eindrucksvollen Beiträge zur Telekommunikationsbranche erhalten hat.