Technology-shutterstock_1473153593

As IoT and smart buildings continue to converge, more devices are being installed outside the traditional method, such as in areas above the ceiling or on the wall. Some good examples of this include wireless access points, PoE LED lighting systems, AV displays (SDVoE or HDBaseT) and surveillance cameras. Today, these devices are designed with built-in RJ45 ports.

 

As technology changes, so does the way we install these devices. As we’ve shared a few times in recent blogs, TIA recently approved a new topology known as modular plug terminated link (MPTL), or what we like to call “direct connect.” This topology allows the horizontal cable to be terminated on one end to an RJ45 plug that connects directly to a device.

 

So what benefits does direct connect offer? Several!

 

1. Direct Connect Simplifies Installation

First, it eliminates the outlet, jack and patch cord – so it requires fewer components for installation. You no longer have to terminate cable to outlets, install a faceplate or connect a patch cord. This reduces overall installation costs and means that devices can be installed faster.

 

2. Direct Connect Supports Above-Ceiling Applications

It simplifies device installation in above-ceiling applications where faceplate installation isn’t practical – or where outlets, jacks and patch cords must be plenum rated. Instead, you can use a custom-length, plenum-rated cable with plenum-rated plug to connect directly to the end device you’re installing.

 

3. Direct Connect with a FlexPlug is Safer

When patch cords are left exposed, they can be disconnected (whether on accident or on purpose). It’s as simple as pulling the cord out of the device. This could create a security concern, especially if devices like surveillance cameras or PoE LED lighting fixtures are disconnected.

 

Using direct connect with a FlexPlug allows all connections to be out of sight in the ceiling or within the device, making it more difficult to disconnect the device.

 

4. Direct Connect Looks Better

By eliminating outlets and patch cords, you create a cleaner, neater appearance. This may not be a factor to consider in some applications, but in venues like hospitality environments and entertainment settings, employees and guests will no longer be able to see cords stretching from a device to an outlet.

 

Testing for MPTL/Direct Connect

This topology isn’t necessarily a new idea. Belden supports this topology with permanent link testing using the AX104552 test coupler. Now, the rest of the industry agrees that this is a good idea. The ANSI/TIA-568.2-D standard includes the MPTL configuration, as well as a test procedure that includes the final plug connection at the far end. This allows you to verify the performance of the entire connection.

 

Belden’s REVConnect Connectivity System works well for direct connect. Supporting the MPTL topology, REVConnect uses a single termination process for every application. It offers a complete connectivity solution for Category 5e, 6 and 6A shielded and unshielded cable, allowing you to switch from a jack to a plug – or vice versa – without having to re-terminate.

Über den Autor

Ron Tellas

Senior Solution Architect, Enterprise Solutions, Belden

Ron Tellas ist Fachexperte für HF-Design und elektromagnetische Ausbreitung. Er hat sich Belden im Jahr 2016 angeschlossen, um mitzuhelfen, den Zeitplan für Technologien und Anwendungen im Bereich intelligente Gebäude mitzugestalten. Dank dieser Erfahrungen kann er heute sehr effektiv Systeme, Geräte und Verbindungstechnik in Netzwerklösungen integrieren. Ron Tellas vertritt Belden in mehreren Standardisierungsorganisationen, Ausschüssen des National Electrical Code und als Vorstandsmitglied der FMP Alliance. Er hat einen Master- und Bachelor-Abschluss in Elektrotechnik und einen Master-Abschluss in Betriebswirtschaftslehre erworben und hat 17 US-Patente angemeldet. Er ist stolzer Empfänger des 2024 Harry J. Pfister Award, einer Auszeichnung, die er für seine herausragenden und eindrucksvollen Beiträge zur Telekommunikationsbranche erhalten hat.