As fiber continues to move into the mainstream, managing your fiber projects to achieve the outcomes that you—and your client—expect will be vital. You need to be ready to design, install and manage fiber effectively.
And we’ve learned a little trick to make it easier. Want in on the secret?
It starts with creating a fiber playbook. There is no single fiber solution that will meet all your needs, which is what makes a fiber playbook so helpful.
What’s a fiber project playbook?
Think of a playbook as a roadmap—a diary of trust that spells out how you’ll achieve expected outcomes based on needs and the constraints of your environment.
When you build it right, your fiber playbook will empower you to do the following:
- Capture all the requirements you need to get through your fiber project successfully.
- Document and ensure that everyone’s goals are met throughout the fiber project.
- Provide a way to record, formalize, organize and regularly review all the fiber “plays” and strategies your project team can use, along with their impacts.
- Reduce the amount of time you spend in firefighter mode so you can focus on your job without worrying about as many unexpected emergencies or troubleshooting issues.
- Develop a framework for succession planning. Even if the playbook won’t be relevant to your role in five or 10 years, it will be very valuable to whoever comes in behind you and needs this information.
A fiber playbook isn’t just a guide for the pre-planning phase of design, but for everything involved with your fiber. It helps you lay out system requirements and practical solutions to visualize your target and what you need to achieve success.
What information should we include?
At a high level, it should include information about:
- People
- Organizations
- Processes
- Materials, tools and other technologies
It can include pictures, diagrams, examples, and even links for firmware updates and technology resources.
Here are some vital components to include in every fiber playbook you create:
- A description of the organization’s needs. What’s driving this need? Why is the need there in the first place? Why must it be addressed? While standards can play a role, you may have to go beyond the standards to achieve what you truly need.
- The people and organizations that will be impacted. Who will be served by this fiber solution? Who will be involved in the project, and what role will they play? This section should include clients, agents, vendors, channel partners, contractors and consultants.
- Processes. Record things like workflows, installation practices, trusted resources, formulas, expected performance levels, maintenance tasks and troubleshooting steps.
- Materials and tools. This section should include documentation of components and equipment, pictures, examples, software and testing gear. Be clear in the language you use so that anyone who picks up the playbook will know exactly which component or piece of equipment you’re referring to.
- Technologies and other resources. This can involve things like monitoring, security and asset management, as well as the coordination required for these resources.
- Erwartete Ergebnisse. Welche Ergebnisse erwarten Sie? Wie wird der Erfolg gemessen und verifiziert? Welche Leistungswerte werden priorisiert und wie werden diese Werte dokumentiert?
Wie oft sollten wir unser Glasfaser-Playbook aktualisieren?
So wie sich das Spielbuch einer Fußballmannschaft von Saison zu Saison ändert, ändert sich auch das Spielbuch Ihres Glasfaserprojekts je nach den Entwicklungen in der Technologie, den Geschäftsanforderungen, Ihrer Umgebung und sogar den Ereignissen weltweit.’’—’ Fragen Sie einfach jeden, der ein Glasfaserprojekt-Playbook verwaltete, als die Pandemie ausbrach, als der Bundesstaat Texas einen noch nie dagewesenen Frost erlebte oder als ein 5G-Turm in England in Brand gesteckt wurde: Änderungen werden notwendig sein!
Beispielsweise haben Sie vor 20 Jahren vielleicht OM1-Faser zum Anschließen von Schalttafeln verwendet. Doch mit der zunehmenden Ethernet-Geschwindigkeit kann die OM1-Glasfaser’nicht Schritt halten. Ihre interne Spezifikation oder Norm muss sich ebenfalls ändern.
Betrachten Sie zum Beispiel ein Rechenzentrum. Wir haben mit einem Kunden zusammengearbeitet, um ihn bei der Aktualisierung seines Glasfaser-Playbooks während der Modernisierung seines Datenzentrums zu unterstützen. Das Playbook enthielt natürlich Informationen über Glasfaser, aber es enthielt auch Informationen über neue End-of-Row-Methoden und wie sie Geräte- und Technologie-Migrationen verwalten.
Der nächste Schritt beim Aufbau eines Glasfaser-Playbooks
Da sich die gesamte Welt über das Internet der Dinge vernetzt, um die Automatisierung und datengesteuerte Entscheidungsfindung zu unterstützen, wird eine anpassungsfähige und zielgerichtete Glasfasertechnologie entscheidend sein, um dies zu erreichen.
Sobald Sie wissen, was Sie brauchen (und warum Sie es brauchen)—und die Überlegungen zum Glasfaserdesign und -einsatz besser verstehen—,’sind Sie bereit, Ihr ganz eigenes Glasfaser-Playbook zu entwickeln.
Passende Ressourcen:
- Erstellen eines Glasfaser-Playbooks vom Kontrollraum bis zum Datenzentrum
- Warum Sie diese Alternative zu herkömmlichen metallgepanzerten Fasern in Betracht ziehen sollten
- Singlemode- oder Multimode-Faser: Aufschlüsselung der Unterschiede
Über den Autor
Henry Franc
Field Applications Engineer
Mit seinem Schwerpunkt auf der Konzeption, Planung und dem Bau von Rechenzentren fungiert Henry Franc als vertrauenswürdiger Berater für große oder komplexe Projekte in allen Branchen. Er bewertet die Geschäftsanforderungen der Kunden und findet die besten Technologieoptionen, um diese zu erfüllen. Außerdem wurde er von seinen Branchenkollegen zum stellvertretenden Vorsitzenden des TR42 Telecommunications Cabling Systems Engineering Committee gewählt.